Failed to call pILiveData error when editing Schedule object in Continuum 1.94.

Issue

After upgrading to Continuum 1.94, Cyberstation throws the following error. 

Failed to call pILiveData -> GetLiveData().  ACDataServices has an error.

Product Line

Andover Continuum

Environment

Continuum 1.94

Schedule

Error

Cause

This behaviour is due to a bug that was described in TPA-BOST-12-0002 00 Schedule Exception Errors.

Resolution

Install the Hotfix for TPA-CONT-12-0002.00_Schedule_Exception_Errors which can be found on the Buildings Business Extranet.