Will the DSSRV ethernet port power an IP camera?

Issue

Will the second ethernet port on the DSSRV power an IP camera?

Product Line

Pelco Video Management

Environment

DSSRV POE IP CAMERA

Cause

Will the DSSRV power an IP camera?

Resolution

No. A power source - POE injector or POE switch will be needed.

Check the install manual for the IP camera for further information.

See Lessons Learned Article #10073 for part number information.