How to install the DX8100-EXP.

DANGER

HAZARD OF ELECTRIC SHOCK.
Remove all power from all devices before removing any covers or doors of the system. Disconnect the power at the device and at the power source.

WARNING

ELECTROSTATIC DISCHARGE REQUIRED.
Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Installation of the DX8100-EXP card.

Product Line

Pelco Video Management

Environment

  • DX8100
  • DX8100-EXP

Cause

Installation of I/O card for the DX8100-EXP.

Resolution

Install the DX8100 I/O Card

To install the DX8100 I/O card in slot 7:

1. Remove the Rear Cross Brace.

2. Do the following:

      a. Remove the slot cover for slot 7 and retain the screw.

      b. Insert the DX8100 I/O card into the slot 7 opening and secure the I/O card bracket with the screw.

      c. Insert the 4-wire DX8100 power plug into the I/O card power connector CN302.

      d. Insert the 5-pin Alarm and Relay cable into the DX8100 I/O card Alarm and Relay connector CN303. The other end of the cable inserts into the optional Capture Card.

      e. Insert the 32-pin ribbon cable into the video connector CN304.

3. This completes installation of the DX8100 I/O card.

Capture Card

Installing the Optional Capture Card

To install the optional Capture Card:

1. On the main Capture Card, remove the 7-wire TV/Audio cable and lay the cable over the DX8100 I/O card. Refer to below image for the location of the TV/Audio cable.

2. Do the following:

      a. Remove the slot cover for slot 3 and retain the screw.

      b. Place the optional Capture Card under the 5-wire Alarm and Relay cable from the main Alarm and Relay I/O board and firmly seat the card in the PCI slot 3 connector, and then secure the Capture Card bracket with the screw.

      c. Connect the 7-wire TV/Audio cable to the TV/Audio connector on the optional and main Capture Card.

      d. Verify that the 5-wire Alarm and Relay cable from the main Alarm and Relay I/O board is firmly inserted in the I/O connector on the main Capture Card.

      e. Connect the 5-wire Alarm and Relay cable from the DX8100 I/O card to the I/O connector on the optional Capture Card.

      f. Connect the 32-pin ribbon cable from the DX8100 I/O card to the second video connector on the optional Capture Card.

      g. Insert the 14-pin ribbon cable into the PB-Path connectors on the optional, and then main Capture Card.

      h. This completes installation of the Capture Card.

Optional

 

DX8100 Expansion parts list:

For more information on installing the DX8100-EXP refer to the DX8100-EXP Expansion Unit Installation Manual.