Can the DX Series Client perform PTZ functions on the DX units?

Issue

PTZ control from the DX Series Client.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • DX4000 Series DVR
  • DX4100 Series DVR
  • DX4500 / DX4600 Series DVR
  • DX4700 / DX4800 Series HVR
  • DX8000 Series DVR
  • DX8100 Series HVR
  • Windows 7

Cause

Verifying DX Series capabilities.

Resolution

Yes, the DX series client is able to perform PTZ functions on the DX units.

NOTE: Once DX Series Client establishes remote connection to the DX unit; the user must right click on the DX DVR and select user login. After login in with the user account that allows PTZ control, the user will be able to get PTZ control of the camera.