Can I Access the PTZ Camera Programming Menu using the DX7100 DVR?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Accessing to the pelco PTZ camera menu through DX7100 DVR

Product Line

Pelco Cameras

Environment

  • Pelco PTZ Cameras
  • DX7100 Series DVR

Cause

95 Preset Command

Resolution

The Preset 95 command is not supported on the DX7100 controls. Spectra® or Esprit® programming menus can be accessed through preset 95 with a KBD200A or KBD300A keyboard in the direct mode.