Will the DX4800HD support alarm recording for IP cameras?

Issue

DX4800HD is not recording alarms from IP cameras.

Product Line

Pelco Video Management

Environment

  • DX4700/DX4800 (HD)
  • Pelco IP cameras
    • Note: Oncam Grandeye 360 camera is not supported.
    • version 2.0.1.00.0869, Onvif is only support for Pro series.
  • Axis Vapix 3 (version 5.x or later)
  • DX4700/DX4800 (nonHD)
    • All Pro series cameras are not supported. (IMP, IMP+, IBP, IBP+, IXP, IJP+, IWP+, P1220)

Cause

Will the DX4700/DX4800 support alarm recording for IP cameras?

Resolution

The unit does not support alarm recording for IP cameras.

For more information see page 40 in the DX4700HD DX4800 HD server configuration