First object in a Sigma IC3-SNP always displays it's default value

Issue

The Sigma object associated with the first entry in the Gateway.txt file of an S-IC3-SNP integration controller when displayed in the Sigma System Manager, always shows its default value.

Product Line

Satchwell Sigma

Environment

Sigma

S-IC3-SNP

Cause

There is an issue with the way that the S-IC3-SNP processes the object mapping file (gateway.txt) file, please note that this issue does not affect the earlier S-IC-SNP

Resolution

TPA-LOND-08-0011.00 provides a workaround for this issue, the work around involves adding a dummy line to the Gateway.txt file, this then allows the first object to be displayed normally.