How to find the TCP/IP or MAC address of the DX4700/DX4800(HD)?

Issue

  • Where do I find the MAC address on the DX4700/DX4800(HD) DVR.
     
  • Where do I find the TCP/IP or DHCP address on the DX4700/DX4800 DVR.

Product Line

Pelco Video Management

Environment

  • DX4104
  • DX4700/DX4800
  • DX4700/DX4800(HD)

Cause

What is the MAC address of a DX4800(HD) DVR?

Resolution

  1. Log on to the DVR as the Admin. The default admin password is admin.
  2. Click on the " (I) " icon on the menu bar and the MAC address will be listed in the information page.

NOTE: You cannot get the MAC address from the client software. It has to be obtained from the server itself.