DS Xpress, DSRealVue, DS1000 hard drive part numbers.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

The HDD part numbers are not listed for the DS Xpress, DSRealVue or DS1000.

Product Line

Pelco Video Management

Environment

DS Xpress, DS RealVUE, DS1000 4.1 through 7.0

Cause

The HD's will eventual fail and need replacing. 

Resolution

The following drives can be used in DigitalSentry systems with P4 or dual core processors.

For 250GB hard drive replacements use EE08-3250-6204G
For 500GB hard drive replacements use EE08-3500-6203G

The following drives can only be used in DigitalSentry systems with dual core processors. Max of 4TB total. Example: qty. 2, 2TB drives or qty. 4, 1TB drives.

For 1TB hard drive replacements use EE11-0001-2014
For 2TB hard drive replacements use HDD2000-SVSATA

*For data drives, the disk will need to be formatted and partitioned in Windows.
*For OS drives, a recovery disk will need to be run to install Windows