Issue
After commissioned in Vista Workstation, all the nvi values in the LonWorks device become to default value of in the Vista database.
Environment
Cause
When commissioning LonWorks device in the Vista Workstation, there are three options. In this situation, the option "Download default parameters from XIF file to device” is probably selected.
Resolution
If the nvi value wants to be kept, the “Upload parameters from device to Vista” should be chosen instead of “Download default parameters from XIF file to device”