Database schema upgrade failed

Issue

Database schema upgrade failed

Product Line

TAC Vista

Environment

Vista 5.1.X

taclogdata database SQL 2005/2008

Cause

The error message in the b0warlog suggests this is caused by the automatic database schema upgrade failing.

Resolution

See TAC Vista installation manual section 5.3