Access to the Pelco PTZ 95 Preset Camera Menu through the Dedicated Micros Controller.

Issue

Access to the Pelco PTZ 95 Preset Menu

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Spectra II, III, IV, Spectra MINI, Esprit, Exsite
  • Dedicated Micros Controller

Cause

Access to the Pelco PTZ Cameras Menu through Dedicated Micros Controller

Resolution

To Access the Spectra Dome menu:

1. Press * (Star) button on the Dedicated Micros Controller.

2. Select the Camera menu

3. Press Open (+) to select

Notes: You can also try holding Preset down then press 95 on some Dedicated Micro Controllers as well.


To navigate the Domes  menu using the DS Keyboards:

  1. Use the DS keyboards joystick (up / down) to move the cursor from Line to Line.
     
  2. Press the key to select a menu item.
     
  3. Press the key to cancel.
     
  4. To exit the Domes menu Slect EXIT in the menu and press.
     
  5. The Dome menu will disappear fromt he screen but * will still be at the bottom of the screen.
     
  6. Press and hold down the <* button> to switch the dome menu control off (* disappears).
     

Notes: This process works for MOST Dedicated Micros Controllers.