How to Access the Pelco PTZ Cameras Menu through the Honeywell Controller.

Issue

Access to the Pelco PTZ Cameras Menu through Honeywell Controller

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Spectra II, III, IV, Spectra MINI, Esprit, Exsite
  • Honeywell Controller

Cause

Access to the Pelco PTZ Menu through Honeywell Controller.

Resolution

1. Select the camera on the controller.

2. Select  Maintenance

3. Select Video

4. Select Camera Menu

Notes: This process work for MOST Honeywell Controllers

Another option is to type 9 5 Set

1. Camera menu appears

2. Use joystick to toggle up or down

3. Use Iris Open to enable making a change

4. Once in toggle the joystick up or down to change the variable

5. Iris closed to exit that option

6. Iris closed again to exit menu or toggle to exit and push Iris open