Continuum controller CPU light solid or not illuminated.

Issue

  • Controller is unresponsive and does not respond to a hard reset or power cycle with the battery disconnected.. 
  • CPU light remains on constantly.

Product Line

Andover Continuum

Environment

Continuum

InfinityController

NetController II

CX9680

Cause

Controller stopped functioning after power cycled.

Resolution

  • Test controller with a known working PS power supply. 
  • If the controller still does not respond to a hard reset then return for repair.