BASEDON keyword and PE Programming

Issue

BASEDON keyword and Plain English Programming

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation site with up to release 1.3 

Cause

BASEDON key word fails
Below is a sample program which uses the BASEDON keyword. Also, here are the steps to use that program:
1. Create script program using keyword BASEDON (Below)
2. Create an input and output for the program (below program that is EntreeBase and SortieBase)
3. Set the input Entreebase to 1,2,3,4,5 and program errors out.
4. Set input to 6 and program runs


Numeric Input EntreeBase
Numeric Output SortieBase

Line Debut
basedon Entreebase goto 1,2,3,4,5
goto 6

Line 1
SortieBase=1
goto Suite

Line 2
SortieBase=2
goto Suite

Line 3
SortieBase=3
goto Suite

Line 4
SortieBase=4
goto Suite

Line 5
SortieBase=5
goto Suite

Line 6
Sortiebase=6
goto suite

Line suite
if sortiebase<1 then Sortiebase=20
if ts<5 then goto suite else goto Debut

Line E
Sortiebase=10
goto Suite 


Resolution

BASEDON keyword has been submitted as an issue and expected to be corrected in a future release.