Issue
HID iClass SmartCards can be ordered with 2K, 16K and 32K memory. Which memory amount is required when using BioScrypt iClass readers with the Continuum - BioScrypt integration software?
Environment
CyberStation, BioScript IClass Smart Cards.
Cause
A project requires HID iClass SmartCards, BioScrypt iClass readers and the Continuum - BioScrypt integration software. HID 2K iClass SmartCards do not have enough on-board memory to store fingerprint templates.
Resolution
If you are configuring the BioScrypt iClass readers for the standard 1:1 TEM fingerprint format, you need 16K memory HID iClass SmartCards. If you are configuring the BioScrypt iClass readers for high resolution 1:1 BUR fingerprint format, you need 32K memory HID iClass SmartCards.