Dynamic SNVT in StruxureWare Building Operation.

Issue

Is it possible to use dynamic SNVTs in StruxureWare Building Operation?

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation version 1.3.

Cause

A XIF file including Dynamic SNVTS is often created by a LNS plugin and depending on the settings in the LNS plugin the XIF file changes.
Even when the Xif file changes the program ID in the XIF does not.
And in SmartStruxure it is not possible to import two XIF files with the same program ID.

Resolution

Dynamic SNVT works but only for one device, if different devices have different settings in the LNS plugin only one can be imported.