Issue
Can Modbus TCP and Modbus Async be used simultaneously in an ENC-520?
Environment
I/A Series G3 ENC-520 Modbus Integration
Cause
Modbus TCP integration and Modbus Async integration are both required from a single ENC-520
Resolution
Yes, you can license an ENC-520 for both Modbus TCP and Modbus Async and run them in a single ENC.