Issue
When looking on a TGML graphic from Webstation on a PC the graphics is cached on the PC.
In which folder on the PC is the TGML graphics cached?
Environment
TAC Vista Webstation 5.1.8 and later
Cause
The TGML graphics is cached on the Webstation client PC for faster access. The client don't need to download the graphic from the master every time the graphic is opened.
Resolution
The graphics is cached on this location:
XP:
C:\Documents and Settings\xxx\Local Settings\Temp\Webstation
WIN7:
C:\Users\xxxx\AppData\Local\Temp\Webstation
xxxx=user