CM6800 System Manager

Issue

Where can I find the System Manager?

Product Line

Pelco Matrix

Environment

CM6800

Cause

  • The manager is needed to make changes to the CM6800 programming.
  • All programming is needed to be saved prior to Factory Reset of Matrix.

Resolution

Confirm the software version running on the matrix and match it with the proper version of the manager program.
The version is under the last entry " About CM6800 " in the programming screen on the 6800 matrix.

Related Topics:
How do I connect a computer using Com 1 to the CM6800E-48X8 Matrix
Where Can I Download the CM6800 Matrix Firmware