Keep others from using local TAC Vista IV licenses

Issue

How do you keep others from using my TAC Vista IV licenses?

Product Line

TAC Vista

Environment

Vista IV Licensing

Cause

Networked PCs will look for licenses outside of their local drives. On a shared engineering drive, this can cause problems.

Resolution

In order to have your PC set up so that it does not share its license over a network:

  1. Go to Start > Run > Type in regedit
  2. Click OK
  3. Go to HKEY_LOCAL_MACHINE > SOFTWARE > Aladdin Knowledge Systems > Privilege Licenser > Applications
  4. Click on PLServe
  5. Double click on Network
  6. Change the 1 to a 0