How to access PTZ camera menus using a KBD960

Issue

PTZ 95 Preset menu access.

Product Line

Pelco Cameras, Pelco Matrix

Environment

  • KBD960 - all versions
  • CM6800 - all versions
  • Spectra - all versions
  • Esprit - all versions
  • Exsite - all versions

Cause

Access of 95 Preset Menu to perform advance feature programming of PTZ Camera

Resolution

Using the KBD960, select a PTZ camera and verify that the KBD960 has PTZ control. Press the ESC button until the MAIN MENU appears. 

See LL#10612 for use of KBD300A/KBD200A with CM6800 Matrix.

From the MAIN MENU: