Can the XIF be generated for an AS?

Issue

Can the XIF be generated for an AS?

Product Line

SmartStruxure Solution

Environment

Automation Server

Cause

Want to add AS into another system and need XIF

Resolution

In version 1.4.0 and below the Automation Server can not be integrated into other systems using LonWorks.

From version 1.4.1 and up, you can configure an "Externally Managed LonWorks Network" to the Automation Server, and as a result use the Automation Server in e.g. LonMaker or NL220. The Automation Server supports "Upload from device", but if you need the xif file, you can refer to these two documents.