Fixed ExSite EHXM or EHXME series does not feature the programming option of Unit Inversion.

Issue

  • Programming Menu of Fixed ExSite does not feature the option of "UNIT INVERSION"
  • How to adjust the ExSite position?

Product Line

Pelco Cameras

Environment

  • EHXM3036
  • EHXM3136
  • EHXME036
  • EHXME123

Cause

Mounting Exsite upside down.

Resolution

The Fixed ExSite series is manually adjusted for inversion operation:

  • Pan Adjustment via loosening of Locking Ring
  • Tilt Adjustment via Set Screw, Tilt Shaft and tilt Lock nut.
  • Click Here to view manual adjustment document.