When attempting to build connection to a Filemaster the error invalid I/NET seven operator is given

Issue

When attempting to build connection to a Filemaster the error "invalid I/NET seven operator" is given

Product Line

TAC I/NET

Environment

I/NET

Filemaster Equalized client

Cause

When building a connection to a remote database, you must use the credentials for the remote PC not the local PC. In this example, when creating the connection to a Filemaster from a Equalized client, you must use the I/NET log in credentials for the Filemaster.

Resolution

Change the I/NET user name and password to one that has full permissions on the Filemaster PC.  You may need to attempt to log into the filemaster PC to verify the username and password.