Issue
When a value from a object in one Vista server should be transferred to a object in a value on another Vista server, Is it possible to use object transfer?
Environment
TAC Vista 5.1.x
Cause
In general a minimum of communication between the Vista servers should be used as it is much slower then internal communication within the server itself. But it is possible to do.
Resolution
Yes it is possible to have a object transfer between objects in different Vista server nodes.