Issue
Is there a limit to how much CPU power the graphics editor can utilise?
Environment
Tac Vista 5.1.X
Graphics Editor TGML
Cause
The graphics editor appears to be limited to a maximum of 25% CPU usage, which means that some heavy operations take a long time.
Resolution
There is no limit to how much CPU graphics editor can utilise. However each thread can only use 100% of each CPU core, so a quad-core CPU would allow for a maxim of 25% total CPU usage per thread.