CM9700 Series Matrix Bay Power Supply part number

Issue

What is the part number for a CM9700 (CM9765/70/80) Matrix Bay Power Supply?

Product Line

Pelco Matrix, Pelco Transmission & Power

Environment

CM9700 Matrix Switcher

CM9700-MPS

CM9765-MXB

CM9770-MXB

CM9780-MXB

Cause

Replacement Part

Resolution

The part number for a CM9700 (CM9765/70/80) Matrix Bay Power supply:

CM9700-MPS

 

NOTE: The CM9700-MPS is only for the CM9765/CM9770 and CM9780-MXB's. This power supply is not compatible with the CM9760-MXB or the CM9740-MXB.