Issue
Two Carel BACnet gateways, when connected to the MSTP one at a time then doing 'Find BACnet devices' they show up under the BACnet folder but if connected together they do not.
Environment
CyberStation
bCX4040
Cause
Continuum enhanced MSTP mode is interfering.
Resolution
Disable Continuum enhanced MSTP mode.