DX8100 Partition Software.

Issue

Where can I get the Partition software for my DX8100?

Product Line

Pelco Video Management

Environment

DX8100 Partition Hard drive

Cause

Replacing the master hard drive requires the partition cd to be run before the recovery to set up the MBR and set the C: and D: partition.

Resolution

 

Link to the  DX8100 Partition CD
 

Using windows 7 to create a ISO. bootable disk

  1. Right click on ISO file
  2. Select "Open with"
  3. Select "Windows Disc Image Burner" 
  4. Once done a ghost.exe (Application) will be seen.
     


 

 Note:Recommend CD-R for iso.

Related Articles:
Partitioning the system drive and data disk on the DX8100 Series hybrid video recorder (HVR).