Are CM9740-CC1, CM9750-CC1 and CM9760-CC1 are obsolete?

Issue

What are my options for replacing my CM9740-CC1, CM9750-CC1 or CM9760-CC1 which are obsolete?

Product Line

Pelco Matrix

Environment

CM9740-CC1

CM9740-MXB

CM9760-CC1

CM9760-MXB

CM9740-VCC

CM9740-VMC

Cause

Failed CM9740-VMC, CM9740-VCC and CM9740-CC1 or CM9760-CC1.

Resolution

Replace all CM9740 and CM9760-CC1's with a CM9700-CC1.

NOTE: New CM9700-CC1's are shipped with version 9.03.0xx software. Make sure to replace the executable file with the correct executable version software, prior to importing the existing flat files.