SmartStruxure 1.3 user accounts - Can a user have access to change a value on a Graphic, without access to its other functions?

Issue

Access which allows a value to be changed, also allows other changes to be made.

Product Line

SmartStruxure Solution

Environment

Users

User accounts

Cause

A user account is created to have read only access, but this user must also have access to view Graphics, and on these graphics, be able to change values. How can this be achieved without allowing the user access to delete or edit these objects?
 

Resolution

At StruxureWare Building Operation release 1.3 there are no available options that will achieve this configuration, the most appropriate configuration is to create a Workspace for the user, in which they will see only the Graphics, the user would have Read/Write access to the values they are allowed to change.