Issue
After installing Tree Tech 3.2 on a Windows 7, 32-bit computer and creating a new project, I am not able to Add an object or segment to it; in the File, Add menu, Object and Segment are grayed-out.
Environment
Tree Tech 3.2
Windows 7, 32-bit computer
Cause
Not yet determined
Resolution
1. Close Tree Tech 3.2 and any other running programs.
2. Shut down & restart the computer.
3. From the desktop icon, double-click on "Run Tree" to start Tree Tech.
4. Open the project created earlier. From the File, Add menu, the Object and Segment should no longer be grayed-out.