Warning
Potential for Data Loss: The steps detailed in the resolution of this article may result in a loss of critical data if not performed properly. Before beginning these steps, make sure all important data is backed up in the event of data loss. If you are unsure or unfamiliar with any complex steps detailed in this article, please contact Product Support Services for assistance.
Issue
Error 'Operation was not performed' when trying to run a Graphic object.
Environment
CyberStation
Cause
Corrupted Continuum installation
Resolution
Uninstall Continuum
Delete Continuum folder (make sure to save any needed files such as pin, menu etc)
Delete Continuum entries in the registry (Make sure to backup registry as a precaution)
HKEY_CURRENT_USER\Software\Andover Controls\Continuum
HKEY_LOCAL_MACHINE\SOFTWARE\Andover Controls\Continuum
Re-install Continuum