Where can I download the latest version of the DX Series Client?

Issue

  • Where can I download the DX Series Client?
  • Need to know what is the latest DX Series Client software available.

Product Line

Pelco Video Management

Environment

  • DX Series Client  software compatible with:
    • DX4100 Series
    • DX4500/DX4600 Series
    • DX4700/DX4800 Series
    • DX4700HD/DX4800HD Series 
    • DX8000 Series
    • DX8100 Series
    • Windows 7
    • Windows 8

Cause

Update DX Series Client to the latest released version.

Resolution

To download the latest version of the DX Series Client click HERE

  1. Locate the latest software release (example: DX Series Client Installer ver 2.1.0.0044)
  2. Click on the link to download. (The file is in a .ZIP format, make sure to extract before attempting installation).


NOTE:
Local Administration rights are needed to install, configured and use DX4500_4600 client.
Adding the client to a system requires populating the camera view pane with camera views.

Previous DX Series Client software versions can be download as needed. 

Click on the following to download DX_Series_Client_Installer(ver2.0.1.0036).zip

Click on the following to download DX_Series_Client_Installer(ver 1.0.1.0010).exe