How to increase the number of modbus registers the Xenta server polls in a single request

Issue

How do I increase the number of modbus registers the Xenta server polls in a single request?

Product Line

TAC Vista

Environment

XBuilder
Xenta 511
Xenta 913
Xenta 701
Xenta 711
Xenta 721
Xenta 731

Cause

This feature is not well documented in the Xenta 700 documentation, though it is mentioned in the TAC Xenta Server – Gateway, Technical Manual (Xenta 913).

Resolution

This feature is not well documented in the Xenta 700 documentation, though it is mentioned in the TAC Xenta Server – Gateway, Technical Manual (Xenta 913).