What is the part number of the over molded cable for the EPS5000-120?

Issue

Replacement part Over Molded Cable. The 6-pin power connector allows you to connect an over-molded cable from the EPS5000-120 to either the RK5000-3U or the RK5000PS-3U.

Product Line

Pelco Transmission & Power

Environment

EPS5000-120 - all versions.

RK5000-3U - all versions.

RK5000PS-3U - all versions.

Cause

Installation, and Maintenance.

Resolution

The EPS5000-120 can be used in the following ways:

  • Provide power to two fully populated RK5000-3U
  • Provide power to one fully populated RK5000-3U
  • Provide redundant power to one fully populated RK5000PS-3U
  • Provide redundant power to two fully populated RK5000PS-3U

*Note

Two snap-on ferrites are supplied with the EPS5000-120 external power supply, one for each over-molded cable. Each ferrite must be attached to the end of the over-molded cable that plugs into either an RK5000-3U or RK5000PS-3U. The ferrites must be attached to the over-molded cables for the external power supply to comply with FCC and CE emissions requirements.

The part number is subject to change so please verify before an order is placed.

The Part Number for the supplied Over-Molded Cable is:  WA01-4884-011AG

The Part Number for the supplied snap-on ferrite for the Over-Molded cable is: XF06-3202-0181