Issue
On a jobsite doing a backup of a GCM and its ASD controllers. After an upload of the GCM is complete, the ASD controllers appear in the tree (the upload of the GCM created them). Do they also need to be uploaded individually?
Product Line
TAC I/A Series
Environment
TreeTech (any version)
Cause
Understanding all the steps in a proper / complete upload of a GCM and its controllers.
Resolution
The first step is to upload the GCM.
The second step is to upload each individual ASD controller (Microzone II, Microflo II, etc...). Each upload will take less than a minute.