Issue
How to retrieve the XBuilder project (XPB) from the Vista Database.
Environment
XBuilder
Xenta Server 913
Xenta Server 511
Xenta Server 7xx
Cause
XBuilder file was not saved and backup was not set to target.
Except Vista database backup do not have any other backups.
Resolution
To manually extract the XBuilder project from the Vista Database follow these steps:
- Using Windows Explorer navigate to the Vista database folder which has the XBuilder project you wish to extract.
- Open the $thisfil folder.
- You can see a zip folder named something like DE03xxxx.ZIP or similar.
- Copy the zip file and paste it in the desired location.
- Unzip this file. The Zip contains the complete XBuilder project inside it.