Object type Specified is invalid when exporting points.

Issue

When using Send to Text to export controller points to a text dump, some points are followed by the following error.

VidioId - The object type specified is invalid.

Product Line

Andover Continuum

Environment

  • Video
  • Export
  • Send to Text

Cause

These errors are usually caused by is a “null” value primed in the DB for those attributes

Resolution

These errors are benign and should be disregarded.

See also Lessons Learned Article #4552.