Issue
Photos are taken with a webcam, saved as JPG and loaded from the file into the personnel record. Was working fine previously. Now they are being stretched (distorted) when added to the personnel records.
Environment
CyberStation with Badging Option, webcam
Cause
In Make/Edit Badge >> Capture >> Options the checkmark had been removed from the "Allow cropping" checkbox. Since the photo dimensions were wider than high, the resulting un-cropped photo had white space above and below it in the Make/Edit Badge screen and when that screen was saved (using the OK button) the image was stretched to fill the photo field in Continuum.
Resolution
In Make/Edit Badge >> Capture >> Options add the checkmark from the "Allow cropping" checkbox.