The new Esprit SE-IP does not support audio

Issue

The new Esprit SE IP does not support audio and has no place for the speaker or microphone on it. The web UI is standard Sarix and shows it on the tabs even though there is no ability for it

Product Line

Pelco Cameras, Pelco Video Management

Environment

Esprit SE-IP

audio set up

Cause

There is no connections on the Esprit SE-IP or firmware set up for audio on the unit.

Resolution

There is no resolution at this time, if audio is needed they will have to choose a different model camera