Issue
Condensation buildup is caused by an enclosures inability to compensate for moisture.
Product Line
Pelco Cameras
Environment
Camera enclosures - all models
Integrated camera systems - all models
Cause
Installation, maintenance.
Resolution
An application may experience excessive humidity or moisture build up from any environmental condition.
- Be sure the correct enclosure is selected for the environment of the application.
- Verify the installation is sealed using clear caulking.
- In some environments moisture is beyond compensation; use bags of Desiccant or Silica Gel.
Outdoor enclosures usually have options for blowers, heaters, and defrosters that can compensate for most environmental conditions. Be sure an indoor unit is NOT used due to the fact that these devices do not have environmental compensations.