Does the camclosure II provide conduit access when surface mounting?

Issue

Unclear documentation on specification sheets; does the Camclosure II provide conduit options when surface mounting?

Product Line

Pelco Cameras

Environment

IS50/51 surface mount - all models

Cause

Sales, Installation, and Service.

Resolution

Only the IS50/51 Series camclosure II models provide conduit access holes when surface mounting.  The IS20/21 does not.

Located on the Mounting Base  the Surface Ring has one wall access, and one side access.

When installing the camera using conduit, the female thread on the mounting base conforms to ANSI  NPSM
(parallel pipe threads), 0.75-inch.