Digital Sentry 3rd party IP Camera audio support.

Issue

  • Unable to record audio using an older Axis IP camera.
  • DS Controlpoint Video export fails.

Product Line

Pelco Video Management

Environment

  • Digital Sentry software version 7.2.30 and above
  • DSSRV / DSSRV2
  • DS NVs
  • Pelco IP cameras
    • Sarix / Spectra / Esprit / NET5x
    • Oncam Grandeye EVO05 / EVO12

Cause

Third party IP camera audio is not supported by the Digital Sentry software.

Resolution

Digital Sentry supports audio streaming / recording from Pelco IP Cameras only, this includes the Oncam Grandeye Evolution cameras (EVO05 / EVO12).  Audio streaming is not supported for 3rd party IP cameras.

 

Note: The Digital Sentry ONVIF IP camera driver does not support audio.