Third party software on my I/NET PC

Issue

Can I run third party software on my I/NET PC

Product Line

TAC I/NET

Environment

I/NET Site

Cause

Third party software on same pc as I/NET

Resolution

TAC software is delivered for use on IBM and compatible PCs. While your PC is capable of running other third party software while running I/NET, trying to do so may present general operational difficulties. This is particularly true if the other third party software is memory resident. When used as it is intended, the TAC software is also memory resident. The use of more than one memory resident program at the same time may impose unresolvable PC system parameter conflicts and may cause one or more of the memory resident programs to fail. Refer to TCON 300.