Issue
It is possible to use Thermistor Inputs in Xenta 281
Product Line
TAC Vista
Environment
Xenta 281
Thermistor Inputs
Cause
The Xenta 281 does not have any special thermistor inputs.
Resolution
Yes, it is possible to use the Xenta 281 Universal Inputs for Thermistor Inputs.
Click HERE to see the procedure.