What versions of Microsoft Windows OS does the DS NVs software support?

Issue

  • DS NVs compatibility with Microsoft Windows 8 and 10 operating system.
  • Does DigitalSentry NVS support Windows Server 2012 R2?

Product Line

Pelco Video Management

Environment

  • DS NVS
  • DS ControlPoint software
  • Microsoft Windows

Cause

  • The Digital Sentry software is currently not compatible with Windows 8 or 10.
  • Installation of DigitalSentry software fails to install on a Windows Server 2012 R2 platform.

Resolution

DS NVs v7.17.136



DS NVs v7.16

Supported Microsoft Operating Systems:

  • Windows Server 2012 R2 32 or 64 bit
  • Windows Server 2008 SP2 32 or 64 bit
  • Windows Server 2003 SP2 32 bit
  • Windows 7 Ultimate 32 or 64 bit
  • Windows 7 Professional 32 or 64 bit

 

DS NVs v7.15 and lower

Supported Microsoft Operating Systems:

  • Windows Server 2008 SP2 32 or 64 bit
  • Windows Server 2003 SP2 32 bit
  • Windows 7 Ultimate 32 or 64 bit
  • Windows 7 Professional 32 or 64 bit
  • Windows Vista SP2 32 or 64 bit
  • Windows XP SP3 32 bit

 

DS ControlPoint is support on all Microsoft Windows versions excepet Windows 8. DS ControlPoint v7.15 and later supports Windows 10.

 

Related Articles:

For the latest DS NVs specification sheet please refer to - DS NVs Specification Sheet

Where can I find the latest Digital Sentry Release Notes?