How to setup Seven Trends

Issue

How do I set up Seven Trends?

Product Line

TAC I/NET

Environment

I/NET site

Cause

How to setup Seven Trends

Resolution

I recommend you read about this in TCON 299 (INET Seven System Operator Guide). The overall sequence for using the SevenTrends features of I/NET Seven is as follows:

  1. Configure DCUs to collect data.
  2. Define trends in host stations to receive data.
  3. Configure host stations to receive collected data.
  4. Set transfer parameters.
  5. Archive SevenTrends data.
  6. Create SevenTrends reports (may be done any time after Step 3 is complete). 

Refer to the SevenReports help file for more information on creating reports.