Error while creating the Continuum DataBase in 64-bit Operating System.

Issue

Error while creating the Continuum DataBase in 64-bit Operating System. SQL Server Installation Package cannot be opened.

                          

Product Line

Andover Continuum

Environment

Continuum 1.93 and below

32-bit Operating Systems

Cause

Continuum 1.93 and below versions do not support in 64-bit Operating Systems.

Resolution

Install Continuum in a supported Operating System.

Read and follow the Continuum compatibility matrix before installing.

 

Download the Andover Continuum Compatibility from the below article:

http://buildingskb.schneider-electric.com/view.php?AID=4240